• No : 23639
  • Release Date : 2018/09/14 15:10
  • Print

Output check

I want to check the output wiring from the servo amplifier. How can I check the wiring without setting the servo amplifier to RD (Ready) status, etc.?
Category : 

Answer

Using MR Configurator2, you can switch the output signals on/off forcibly independently of the servo status. This function is used for output signal wiring check, etc.
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MR Configurator2