• No : 23641
  • Release Date : 2018/09/14 15:10
  • Print

Motor-less operation

Can I debug only by the servo amplifier without connecting the servo motor?
Category : 

Answer

The servo amplifier has the motor-less operation function.
Without connecting the servo motor, output signals or status display can be provided in response to the input device as if the servo motor is actually running. This operation can be used to check the sequence of a controller, etc.
Some models such as linear servo motor are not supported for this operation. Refer to the instruction manual.
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MR Configurator2