• No : 25225
  • Release Date : 2019/09/02 16:01
  • Print

Regarding failure of automatic restart when Windows of MI5122-VW is frozen

MI5122-VW's Windows was frozen but Windows did not restart automatically. What could be the cause?
Category : 

Answer

Windows automatic restart function runs when Windows stops due to the blue screen of Windows.
Even if Windows is frozen on the display, the Windows system may continue to operate.
In that case, Windows automatic restart Function does not run.
Product Name
MELIPC
Series
MI5000