• No : 38009
  • Release Date : 2020/11/12 13:03
  • Print

[EcoMonitorPlus] Caution when you are using Display Unit (Model: EMU4-D65) manufactured in October 2016 or before

What is the caution that must be followed when we are using Display Unit (Model: EMU4-D65) manufactured in October 2016 or before?
Category : 

Answer

Display Unit (Model: EMU4-D65) manufactured in October 2016 or before is version A, S/W version: 1.05, which does not support either Pulse Input Unit (Model: EMU4-PX4) or Analog Input Unit (Model: EMU4-AX4).
For more information, refer to the user's manual of each product. You can download it from MITSUBISHI ELECTRIC FA Global Website.
*Any Display Unit (Model: EMU4-D65) manufactured in November or after is version B.
To check the product version, refer to the following illustration.
 
 
Depending on the product version, the following window will be displayed.
If you would like to consult about upgrading the version, please contact our sales representative.
Product Name
Small Type Display Unit for Energy Measuring Unit
Series
EcoMonitorPlus