• No : 39311
  • Release Date : 2023/02/14 08:54
  • Print

Regarding program execution using SD Memory Cards

Is it possible to execute programs from an SD memory card installed in the FX5 CPU module?
Category : 

Answer

It's possible. Use the boot operation function of the SD memory card.
*To use the boot operation function with the FX5S CPU module, you need to install an additional SD memory card unit: FX5-SDCD.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Option
Series
MELSEC iQ-F Series