• No : 40046
  • Release Date : 2023/08/24 16:14
  • Print

Regarding FX5U/FX5UC CPU Module Built-in functions

When comparing the internal functions of the CPU Modules of the FX5S/FX5UJ and the FX5U/FX5UC, are there any functions supported only by the FX5U/FX5UC CPU Modules?
Category : 

Answer

The functions supported only by the FX5U/FX5UC CPU Modules are listed below.
・Heating and Cooling PID Function
・Positioning communication protocol support function
・Optional battery: FX3U-32BL connection (Battery adds latch area, retains clock data)
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series