• No : 40047
  • Release Date : 2023/08/24 16:30
  • Update : 2024/05/09 09:59
  • Print

Regarding enclosed power cable for input module and input/output module for extension connector type

Which product is included with the power cable FX2NC-100BPCB for the input module and input/output module for extension connector type?
Category : 

Answer

The FX2NC-100BPCB is included with the following products.

CPU Modules: FX5UC-32 MT/D, FX5UC-64 MT/D, FX5UC-96 MT/D
Product Name
FX5UC
Product Category
CPU Module
Series
MELSEC iQ-F Series