• No : 44330
  • Release Date : 2024/03/20 12:56
  • Print

Regarding forced ON/OFF function for external input/output

Is it possible to force X/Y devices to turn ON/OFF from GX Works3?
Category : 

Answer

The "Forced ON/OFF function for external input/output" that forces X/Y devices to turn on/off from GX Works3 is supported with the following firmware versions.
・FX5U/FX5UC CPU Module Ver. 1.300 or later
・FX5UJ CPU Module Ver. 1.060 or later
・FX5S CPU Module Ver. 1.020 or later
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series