The following restrictions apply to the external input/output forced ON/OFF function.
・Since RUN contact setting is RUN/STOP by external signal, forced ON/OFF is disabled.
・If the high-speed I/O function and the forced ON/OFF function for external I/O are executed simultaneously, the forced ON/OFF function is applied while the output conditions of the high-speed I/O function are not satisfied. The applicable high-speed I/O functions are as follows.
① High-speed counter function
32 bit data comparison set (DHSCS instruction)
32 bit data comparison reset (DHSCR instruction)
32 bit data band comparison (DHSZ instruction)
② PWM function
Pulse width modulation (PWM/DPWM instruction)
③ Positioning control function
Pulse output (PLSY/DPLSY instruction)
Mechanical OPR (DSZR/DDSZR instruction)
Relative positioning (DRVI/DDRVI instructions)
Absolute positioning (DRVA/DDRVA instructions)
Interrupt 1-speed positioning (DVIT/DDVIT instruction)
Variable speed operation (PLSV/DPLSV instruction)
Single-table operation (TBL instruction)
Multiple-table operation (DRVTBL instruction)
Multi-axis table operation (DRVMUL instruction)