Factory Automation

Robot Engneering software (MELFA) MELSOFT RT ToolBox3

MELSOFT RT ToolBox3 introduction

Program creation and total engineering support software.

This is computer software to assist with a range of tasks from system startup through to debugging and operation.
The product line includes [RT ToolBox 3 Pro] that allows robot simulations to be run on a 3D CAD software.

RT ToolBox3 introduction
  • Main functions
    Creating and editing programs
    Checking the operating environment prior to robot installation
    Simulation of robot operations on the computer
    Estimating cycle times
    Debugging when robots are started up
    Monitoring robots states and faults during operations

Page top

RT ToolBox3 operation screen

  • Its features include a ribbon bar, output window and docking pane, making information easier to see and the software easier to use.
  • Operations in the 3D monitor screen have also been updated to make using the screen more intuitive.
RT ToolBox3 operation screen

Page top

RT ToolBox3 Pro

The MELFA Works function can be used in RT ToolBox3 Pro.
MELFA Works, an add-in tool of SolidWorks®, can simulate robot production systems on SolidWorks® and output the data of processing paths on workpieces.*1)
*1) SolidWorks® is a registered trademark of SolidWorks Corp, (USA). An add-in tool is a software program that adds certain functions to application software packages.

RT ToolBox3 Pro screen

Page top

Lineup

Three types are available depending on the installed functions.

(●:Supported / —:Not supported)


Program editing
Parameter setting
Monitoring
functions
Simulation functions,
3D viewer
(Tact times, Layout examinations)
CAD links
(Path generation,
Creation of robot programs (templates))
RT ToolBox3 Pro(*1) ● ● ● ●(*2)
RT ToolBox3 ● ● ● —
RT ToolBox3 mini ● ● — —
*2) Formats that can be loaded into SolidWorks®.

Page top

Windows®-compatible

*Windows is registered trademarks of Microsoft Corporation in the United States and other countries.

  • Windows®11,10

Page top

Related Link

Page top