MELSEC MX Controller MX-F model
Product features -Basic system configuration-

Basic system configuration
The MELSEC MX Controller (MX-F model) can be used with an extension connector type I/O module, MELSEC iQ-F Series expansion adapter and extension module, and intelligent function module.
System configuration example
*1: Future support
*2: The MX-F model (support EtherCAT) has an EtherCAT port instead; system configuration constraints, such as the maximum number of stations, also differ.
*3: The number of virtual axes is not included in the number of controllable axes.
Modules
The following lists the devices that support MELSEC MX Controller (MX-F model).