Factory Automation

MELSEC-F series CC-Link, CC-Link/LT

CC-Link

CC-Link master station

FX3U-16CCL-M

FX3U-16CCL-M

Master block supporting CC-Link V2 that can connect to remote I/O station, remote device station, and intelligent device station.

Order acceptance:
March, 2028
Production discontinuation:
September, 2028

CC-Link intelligent device station

FX3U-64CCL

FX3U-64CCL

Interface block supporting CC-Link V2 that as intelligent device station can use extended cyclic setting and on supported PLC, program transfer and monitoring is possible from master station's other station access function.

Order acceptance:
March, 2028
Production discontinuation:
September, 2028

CC-Link/LT

Built-in CC-Link/LT master

FX3UC-32MT-LT(-2)

FX3UC-32MT-LT(-2)

FX3UC-32MT-LT(-2) has CC-Link/LT master functionality built-in and can reduce wiring costs with reduced wiring.

Order acceptance:
February, 2025
Production discontinuation:
March, 2025

Master station

FX2N-64CL-M

FX2N-64CL-M

Can use CC-Link/LT reduced wiring I/O control.

Order acceptance:
February, 2025
Production discontinuation:
March, 2025

Other station access function

Other station access function

By connecting GX Works2 to FX3 series main unit master station, program write, device monitor, and maintenance is possible to FX3 series connected as intelligent device station.

Settings for Network parameter

In GX Works2, parameters can be easily set for CC-Link settings and remote device station initial settings, and network diagnosis can be performed.

Other station access function

Expansion of control points

By connecting FX3G(C)/FX3U(C) series on CC-Link, number of I/O control points can be expanded.

  • FX3G/FX3GC 128 pts→256 pts
  • FX3U/FX3UC 256 pts→384 pts
Expansion of control points