Human-Machine Interfaces (HMIs)-GOT FA Application Package iQ Monozukuri
Easily introduce IoT technologies to the shop floor
Visualization of operation status improves manufacturing process and productivity
- Incorporating the package into existing equipment makes system implementation easy
- Collectively manage information that used to be managed individually
- Template screens to analyze the equipment status are included
- Remote monitoring is easy with a mobile app
iQ Monozukuri Process Remote Monitoring
iQ Monozukuri Process Remote Monitoring is an application package to easily introduce IoT technologies to the shop floor, collect and visualize information of multiple devices, and collectively manage the information.
Manufacturing process and productivity of the whole production can be improved by analyzing the data displayed on GT SoftGOT2000.
The operation status of the shop floor and the information such as operation logs and alarms can be collected from each device via an on-site GOT.
iQ Monozukuri Process Remote Monitoring
iQ Monozukuri Process Remote Monitoring consists of the Process Remote Monitoring setting tool and an iQ Monozukuri Process Remote Monitoring template project for GT SoftGOT2000 that easily realize "collection, visualization, and management of the information collected from multiple devices."
Process Remote Monitoring setting tool
Process Remote Monitoring setting tool collects and visualizes information of the shop floor. This tool can be used by selecting GOTs (more than one) that have the information to be collected and setting the information needed (such as devices or resource data).
Without specialized knowledge such as programming, information to be displayed in GT SoftGOT2000 can be easily set.
iQ Monozukuri Process Remote Monitoring template project for GT SoftGOT2000
An iQ Monozukuri Process Remote Monitoring template project for GT SoftGOT2000 is the project data (template screens) for GT SoftGOT2000 to visualize information that the Process Remote Monitoring setting tool collected from onsite GOTs. The following screens are included in the project data.
- A screen to monitor information of multiple kinds of equipment in a batch (operation status list, operation status trend graph)
- A screen to extract data that suits demands from resource data (extract resource data)
- A screen to analyze statuses of facilities (XbarR chart, alarm pareto chart)
| Related materials | ||
|---|---|---|
|
|
Easily introduce IoT technologies to the shop floor
Visualization of operation status improves manufacturing process and productivity < Contents > •Incorporating the package into existing equipment makes system implementation easy •Collectively manage information that used to be managed individually •Template screens to analyze the equipment status are included •Remote monitoring is easy with a mobile app |
Created :
Size :
|