Factory Automation

Human Machine Interfaces MELHMI-GOT GT SoftGOT

GOT3000 Compatible HMI Software GT SoftGOT3000

Manage both GOT and production sites from your computer

HMI Software

GT SoftGOT3000 License required*

  • *A license key (for the USB port) is no longer needed. The license is now registered electronically.
What can be done with GOT can also be done on your computer

What can be done with GOT can also be done on your computer

  • Production line monitoring is possible on a computer with a screen equivalent to GOT.
  • Similar to the GOT screen, the screen is created using GT Works3. Furthermore, project data for GOT can be converted for use on different models.
What can be done with GOT can also be done on your computer

Monitor multiple lines integrally

Multi-Channel Connection

  • Information from multiple lines can be checked and centrally monitored on a single computer.
  • One SoftGOT can connect to up to four-channel controllers.
Multi-Channel Connection
With GOT On-Site

Monitor via the same screen as the on-site GOT

  • If there is a GOT on-site, SoftGOT can use the on-site GOT data for remote monitoring.
  • The use of the data from the on-site GOT eliminates the need to create screens for SoftGOT.
SoftGOT-GOT Link