Intelligence and AI Functions MELFA Smart Plus


Coordinated control of additional axis

Coordinated operation between the robot and an additional axis makes it possible for the robot to work on workpieces that exceed its operating range.
Constant speed control (spline interpolation) of the workpiece and continuous operation is now possible.
Workpieces can be assembled precisely and inspected while they are moving.
Example
Sealing and machine work on large-scale workpieces
Using a robot with an RTU allows the robot to work uninterrupted on large-scale workpieces that exceed its operating range.
Linear, circular, and spline interpolation supported.

Supported robots
| Robot Type | Robot controller | RT ToolBox3 |
|---|---|---|
| FR series, CR series | CR800-D/R/Q Ver.A3 or later. | Ver.1.02C or later |
Catalog
Please refer to the catalog for details.