Factory Automation

Intelligence and AI Functions MELFA Smart Plus

MELFA Smart Plus Features

Calibration assistance function

Calibration assistance function

Time-consuming teaching a 2D vision sensor has been automated and accuracy improved.

Type of Calibration assistance function
Function name Usefulness
Automatic calibratio Robot/2D vision sensor integration
Calibration of work coordinates Robots and peripheral devices/jigs
Relative position calibration Robots working with robots

Page top

Automatic calibration

automatic calibration window

Simple set-up and improve accurancy

Time-consuming teaching has been automated and accuracy improved.

  • Automating the teaching process has made set-up easier.
  • Configure settings such as the camera position, FOV, and resolution in the automatic calibration window. Automatic teaching and automatic calibration is possible.
  • With automatic calibration, operating conditions are stabilized and accuracy is increased.

Cameras can be mounted in three positions

Fixed above camera
Fixed below camera
Handeye

Page top

Calibration of work coordinates

Teaching is now automated. This makes calibration of the robot and peripheral devices extremely simple.
Note1) This function can only be used when a 2D vision sensor is used as a hand eye.
Note2) Horizontal articulated robot (4-axis) not supported.

Troublesome teaching work eliminated

Teaching of workpiece coordinates is automated. Set-up time and troublesome work reduced.

Automatic calibration is possible even in environments where the workpiece coordinates and the robot's relative position change.
Easy calibration of robots and pallets installed on automated guided vehicles (AGVs) or carts.

Calibration of work coordinates AGV
Calibration of work coordinates Cart

Page top

Relative position calibration

Relative position calibration

Intricate teaching of the robot is automated. Setting up interference avoidance and collaborative operation is now extremely simple!
Note1) MELFA FR series D type robots not supported.
Note2) Horizontal articulated robot (4-axis) not supported.

Reduce man-hours spent

Reduce man-hours spent improving accuracy and setting up interference avoidance and collaborative operation.
Calibration is automated so that the same work coordinates can be used by multiple robots. Reduce worker errors and workloads.

Example

Two robots used
Collaborative operation
Interference avoidance

Page top

Supported robots

Function name Robot Type Robot controller RT ToolBox3
Automatic calibratio FR series,
CR series
CR800-D/R/Q Ver.A3 or later. Ver.1.00 or later
Calibration of work coordinates RV-FR series,
RV-CR series
(*1)
CR800-D/R/Q Ver.A3 or later.
Relative position calibration RV-FR series (*1) CR800-R/Q Ver.A3 or later.(*2)

*1) Horizontal articulated robot (4-axis) not supported.
*2) D type robots not supported.

Page top

Catalog

Page top

Related Link

Page top