We are an expert group in the field of visual inspections and machine vision system. We are not just a manufacturer. Instead, we are a visual inspection and machine vision system manufacturer that combines knowledge of and experience related to image processing algorithms, optical technology, electronics, and machinery in order to provide comprehensive consulting as a development engineering company.
The VTV-9000mini is a small housing model of the VTV-9000 machine vision system, supporting from 0.3M camera up to 65M, and also offers a high-speed image acquisition model.
< Model Lineup >
By imaging from an angle, defects such as scratches and dents can be seen more clearly.
However, if the image is taken from an angle with a standard camera in the manner of a visual inspection, the captured image will only be partially in focus, making it unsuitable for inspection.
The "Super Focusing camera" is a solution to this problem.
In addition to realizing high-precision inspection, it also contributes to cost reduction at the inspection site.
VTV-QCS is software that can be used to check the VTV-9000 operation status or unify the management of inspection data through a PC via LAN
even when you are not on-site at the FA line.
VDA (ViSCO data analyzer) is a monitoring software tool that is used to make charts (graphs) of the inspection results of a VTV-9000 system connected to a network in real time.
Even after our products are purchased, to ensure the possibility of problem-free operation at the inspection site, we provide private training customized for each customer, including everyone from first-time to experienced users.
Currently, web-based training is also available.