Auto Solution Advance Engineering Company, we are manufacturer and distributor of the National Skill Test Board for PLC, as well as training in PLC electrical equipment assembly level 1-3.
Designed for control system and instrumentation engineering and related engineering
- Used for practicing wiring between the test board and the PLC.
- Program editing required for design engineers and automatic electrical maintenance engineer able to practice.
- Suitable for practicing skills to prepare in the national competence test in the field of electrician electronics and computers Technician controlled by Programmable Logic Controller (PLC)
We provide FA product such as PLC, HMI.
We provide training course such as
- Communication system to connect to computers for use with PLCs
- Configure communication channels to communicate with PLC such as RS232 serial port, Internet port.
- Configuration value to use such as Input, Output, Timer, Counter, Data Memory of PLC.