Update : 2019/12/27
Advent2 Labs Consultation Pte Ltd
Our key business focus is to assist organizations to improve their efficiency in operation management. We use Flexsim Simulation Software to proof of concept, identify cause of operation issues and help customers to justify investments. Our customers are Seagate, Hewlett Packard, REC Solar, Keppel Logistics, DHL, Unilever, Illumina and others. We are authorized distributor for FlexSim Simulation Software for Singapore, Malaysia, Thailand, Philippines, Indonesia and other SEA countries.
Address
20 Kallang Ave, Pico Creative Centre Level 6, Singapore 339411
Website
FlexSim Simulation Software
FlexSim is a 3D discrete simulation software. It is opted as the best discrete simulation software of 2019. FlexSim allows companies to build an emulated model of the real system (such as manufacturing and supply chain system), so that the management can make decision based on the result generated from the simulation. Through the simulation, the management is able to gather information such as throughput, waiting time, WIP, resource utilization and other operation performance indices through tables, charts, graphs and diagrams. Using this information, management is able to make strategic decision about the operation. Through the 3D visualization, besides the management is able to comprehend the operational issues and they are also able to have better chance to get the buy-in from the stakeholder.