Update : 2022/05/18
ViSCO Technologies (Thailand) Co., Ltd.
We are an expert group in the field of visual inspections and machine vision system. We are not just a manufacturer. Instead, we are a visual inspection and machine vision system manufacturer that combines knowledge of and experience related to image processing algorithms, optical technology, electronics, and machinery in order to provide comprehensive consulting as a development engineering company.
Address
54 BB Building 13th floor,Room1313, Sukhumvit21Road(Asoke),
Klongtoey-Nua, Wattana, Bangkok, 10110,THAILAND
VTV-9000mini
The VTV-9000mini is a small housing model of the VTV-9000 machine vision system, supporting from 0.3M camera up to 65M, and also offers a high-speed image acquisition model.
< Model Lineup >
- Standard 4 camera model
- High-speed capture 2 camera model
Super Focusing Cameras 12MP Monochrome
By imaging from an angle, defects such as scratches and dents can be seen more clearly.
However, if the image is taken from an angle with a standard camera in the manner of a visual inspection, the captured image will only be partially in focus, making it unsuitable for inspection.
The "Super Focusing camera" is a solution to this problem.
In addition to realizing high-precision inspection, it also contributes to cost reduction at the inspection site.