Products
MELSOFT VIXIO
- Feature
- Specification
- Standards
- Discontinued
What is MELSOFT VIXIO?
MELSOFT VIXIO is a visual inspection software that allows users to use AI without any specialized knowledge.
Concerns in the inspection process
- Labor shortages increase the burden on inspectors
- Generational changes in inspectors make consistent visual inspection difficult
- Even though inspection is rule-based, overdetection is increasing
We want to implement AI for visual inspection, but we find it challenging due to our lack of AI expertise.
The solution -
Visual Inspection Software
Featuring a high-speed, high-accuracy AI algorithm ideal for factory automation
AI introduction challenge
The limited number of defective product images complicates accuracy improvement. Generating AI models requires extensive image learning, making the process time consuming and inefficient.
With MELSOFT VIXIO
Easily generate AI models with high-speed, high-accuracy AI.
Simple operation settings without programming
AI introduction challenge
Even if an AI model could be generated, specialized programming is required to implement it in the system.
With MELSOFT VIXIO
Easily set up tasks in a flowchart format. Settings from model generation to monitor screen creation can be performed with a single tool.
Easy system construction
All functions necessary to construct an AI visual inspection system can be easily set up without programming.
Setting the overall operation
Point
Set the overall operation flow in a flowchart format.
Camera settings
Point
GigE Vision® Camera settings can be configured in the camera’s various settings.
Settings for communication with programmable controllers *
Point
Easy data exchange with various programmable controllers.
*: For details on the connection method, refer to the operating environment.
Inspection monitor screen
Point
A monitor screen can be created by arranging the display elements of multiple monitors in a dashboard format.
Improved traceability
AI introduction challenge
Ensuring traceability is difficult because different types of data are saved using separate tools.
With MELSOFT VIXIO
Inspection date/time, programmable controller data, captured image, and inspection results are automatically linked and saved together in a group, for easy traceability.
Traceability in coordination with a programmable controller
Automatic linking of manufacturing information and judgment results.
Focus and view the data needed by filtering or searching saved data.
Point Immediate analysis of MELSOFT VIXIO judgment results according to the manufacturing date
Immediate analysis of MELSOFT VIXIO judgment results according to the manufacturing date