Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20812
  • Release Date : 2018/08/22 16:24
  • Print

FR-A8NC

The rotations per minute command is sent from CC-Link by Pr.144 = 108. When 422 rpm is sent, the theoretical value monitored as the setting frequency by the communication is 28.133333..Hz. Is this value rounded up or off?
Category : 

Answer

Two digits after the decimal point are rounded off. 28.139 Hz is rounded down to 28.13 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries