FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800 "Parameter for the communication setting"
FAQ
FR-A800 "Parameter for the communication setting"
Pr.1300 to 1400 are described as "Parameter for the communication setting". For what communication are these parameters used?
- Category :
Answer
These parameters are used for the communication compatible with the communication protocol of the Ethernet IP of the HMS optional circuit board (A8NEIP_2P).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800