Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20831
  • Release Date : 2018/08/22 16:24
  • Print

Frequency search of the FR-A800/FR-F800

What is the frequency search (reduced impact restart) that is performed when Pr.162 (Automatic restart after instantaneous power failure selection) is 3 or 13?
Category : 

Answer

DC voltage is applied when Pr.162 = 0, and AC voltage is applied when Pr.162 = 3 or 13. For the AC, the operation is easier to continue than the DC and the impact can be suppressed. Note that, for both V/F and Advanced magnetic flux vector control, tuning is required and the wiring length is 100 m or less.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries