Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20839
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-E

For the CC-Link IE Field BASIC specification, what is (open specification) written with the number of connectable inverters in the Instruction Manual?
Category : 

Answer

It indicate that the actual number of connectable units differs depending on the master side specification although the maximum number of connectable units on the inverter side is 64. (When the maximum number of connectable units on the master side is less than 64, the maximum number of connectable units on the inverter side is the same as that of the master side.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-E

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries