Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20874
  • Release Date : 2018/08/22 16:24
  • Print

FR-A8TP

In New Product RELEASE, it is described that the encoder power supply of both 12 VDC and 24 VDC can be used for the SF-V5RU. Is it also true for the SF-V5R because its encoder is the same as the SF-V5RU one?
Category : 

Answer

Yes, it is.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries