Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20881
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-E

Is the RS-485 communication possible?
Category : 

Answer

It is not possible because the RS-485 terminal block is not installed. Use the FR-A800 (RS-485 communication type) when performing the RS-485 communication.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-E, FR-F800-E
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?