FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Carrier frequency automatic reducing function
FAQ
Carrier frequency automatic reducing function
Does the carrier frequency automatic reduction function of Pr.260 operate immediately?
- Category :
Answer
The function operates immediately when the current of 85% or higher flows. The limit is canceled when the current becomes 80% or lower.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800