Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20903
  • Release Date : 2018/08/22 16:25
  • Print

Carrier frequency automatic reducing function

Does the carrier frequency automatic reduction function of Pr.260 operate immediately?
Category : 

Answer

The function operates immediately when the current of 85% or higher flows. The limit is canceled when the current becomes 80% or lower.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries