FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > FR-PU07BB
FAQ
FR-PU07BB
I turn OFF the inverter power when an alarm occurs. Can the fault status be held by using the battery mode of the FR-PU07BB even when the power supply is turned OFF?
- Category :
Answer
Because the internal reset processing is performed when the power supply is turned OFF, the fault state cannot be held. The details of the faults are saved in the faults history. Refer to it or prepare an inverter that can supply the control circuit power supply from other circuit, consider the circuit that retains the control circuit power supply.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option