FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Emergency stop function
FAQ
Emergency stop function
It is described that when the emergency stop function (X92) is used, the deceleration stop is performed according to the setting in Pr.815 Torque limit level 2. What happens under V/F control?
- Category :
Answer
The deceleration stop is also performed according to the setting in Pr.815 under V/F control.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800