FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800-R2R
FAQ
FR-A800-R2R
What is the difference in performance between dancer feedback speed control and tension sensor feedback torque control? (How should I choose the appropriate one?) Which should I use for the winding shaft and unwinding shaft, speed control or torque control?
- Category :
Answer
Basically, it depends on machine specifications. Advantage of dancer feedback speed control: Easy control. Small tension can be controlled. Disadvantage: Machine configuration is complicated. Advantage of tension sensor feedback torque control: Machine configuration is simple. Disadvantage: When the tension is small, the influence of the change of the mechanical loss is large and the accuracy is low. When reduction ratio is large, the change of the mechanical loss is large and the accuracy is low.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800