Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21013
  • Release Date : 2018/08/22 16:25
  • Print

Parameter copy to the USB memory

Can I write the USB memory parameter copy file (*.cp1) to the inverter when the power supply specification or capacity is different (such as when replacing the FR-A820 with FR-A840)?
Category : 

Answer

Yes. Writing is available when the power supply specification or capacity is different. Note that setting values of the voltage relation is also overwritten according to the voltage difference (200 V/400 V).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries