FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Safety stop function
FAQ
Safety stop function
There are connection diagrams that the safety relay module is connected to the multiple inverters. How many inverters can be connected to the safety relay module?
- Category :
Answer
Up to three inverters can be connected. When more than four inverters are connected, the inverters may not be recognized because of the voltage drop.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800