Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21069
  • Release Date : 2018/08/22 16:25
  • Print

The number of output terminals

Is the number of output terminals and the terminal function selection same as the F700P?
(For F700P: RUN, SU, IPF, OL, FU, ABC)
Category : 

Answer

The number of terminals: There are the same output terminals as F700P and the following terminals (2 points) are added. Safety: SO, SOC *The terminals SO and SOC are dedicated to the safety. Functions cannot be changed as other terminals.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries