FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > The number of input terminals
FAQ
The number of input terminals
Is the number of input terminals the same as that of the F700P series?
(For F700P: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
(For F700P: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
- Category :
Answer
The number of terminals: There are the same input terminals as F700P and the following terminals (4 points) are added. Safety: SI1, SI2, SIC 24 V power supply: + 24 *The terminals SI1, SI2, and SIC are dedicated to the safety. Functions cannot be changed as other terminals.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800