FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > PLC function
FAQ
PLC function
When Pr.414 is set to "1", Pr.388 is set to "0", and the SQ signal is turned ON from the NET to use the PLC function in the NET, P.RUN. is OFF and PLC function is not enabled. Why is this?
- Category :
Answer
When Pr.414 is set to "1" and Pr.388 is set to "0", the PLC function is not enabled unless both the SQ signal from communication and the SQ signal from the external input terminal are turned ON. When the external SQ signal is always ON, Run/Stop of the PLC function can be performed by turning ON/OFF the communication SQ signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800