Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21073
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

When Pr.414 is set to "1", Pr.388 is set to "0", and the SQ signal is turned ON from the NET to use the PLC function in the NET, P.RUN. is OFF and PLC function is not enabled. Why is this?
Category : 

Answer

When Pr.414 is set to "1" and Pr.388 is set to "0", the PLC function is not enabled unless both the SQ signal from communication and the SQ signal from the external input terminal are turned ON. When the external SQ signal is always ON, Run/Stop of the PLC function can be performed by turning ON/OFF the communication SQ signal.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?