FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > FR-PU07
FAQ
FR-PU07
Can I connect the FR-PU07 to FR-A800/F800 directly?
- Category :
Answer
No. They can be connected with the connection cable (FR-CB20[]). [] indicates cable length (1 m, 3 m, 5 m).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, option