Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21097
  • Release Date : 2018/08/22 16:25
  • Print

24 VDC power supply

What will be available if power is supplied to the 24 VDC power supply terminal?
Category : 

Answer

Power is supplied only to the control power supply, and thus this enables communication, parameter setting through the operation panel or an USB memory device, and operation check of the input/output terminals. * The 24 VDC power supply turns OFF when the main circuit power supply is ON.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?