FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > FR-A800
FAQ
FR-A800
Is the installation compatible with the A700 series? FR-A720-0.4K to 90K, FR-A740-0.4K to 280K, FR-A740-315K to 500K
- Category :
Answer
- The 280K or lower has the installation size compatibility. - The 315K or higher does not have the installation compatibility; because the inverter unit and converter unit are separated. For the details of installation size, refer to the catalog.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800