Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21133
  • Release Date : 2018/08/22 16:26
  • Print

Wiring length

In the Instruction Manual of the FR-A700, it is described that the wiring length between INV and IM should be 100 m or less under Vector control. How about under Real sensorless vector control?
Category : 

Answer

Under Real sensorless vector control, the maximum wiring length is 500 m. Under Vector control with encoder, the maximum wiring length is 100 m.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries