Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21148
  • Release Date : 2018/08/22 16:26
  • Print

FR-HC2

What happens when the FR-DU07 provided with the inverter is used for FR-HC2?
Category : 

Answer

It is not available and "Err" is displayed. When the FR-HC2 dedicated DU (FR-DU07-CNV) is installed to the inverter, "Err" is displayed as well. The FR-PU07 can be used with the FR-HC2 and inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries