Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21157
  • Release Date : 2018/08/22 16:26
  • Print

FR-CV

Is there any problem with the ticking reactor FR-CVL?
Category : 

Answer

The reactor generates a sound during power regeneration, but it is not abnormal. [Reason] The noise from the reactor is caused mainly by the magnetic attractive force and magnetostrictive vibration at the iron core gaps, and magnetostrictive vibration of the silicon copper plate, which are transmitted to the iron core, generating a vibration sound come along with the resolution or reflection.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries