Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21180
  • Release Date : 2018/08/22 16:26
  • Print

Rotation speed display

When the Pr.37 (Speed display) or Pr.144 (Speed setting switchover) is set to change the display to the machine speed or rotation speed, is the display of frequency data saved in the faults history switched to the machine speed or rotation speed?
Category : 

Answer

It is not switched. The frequency at the fault saved in the faults history is always displayed in frequency [Hz].
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries