FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Electronic bypass function
FAQ
Electronic bypass function
Can I manually switch the operation to the commercial power supply operation at an inverter fault?
- Category :
Answer
The operation cannot be manually switched to the commercial power supply operation at an inverter fault. The operation can be automatically switched to the commercial power supply operation at an inverter fault. By setting Pr.138 (Bypass selection at a fault) to "1", the operation is switched to the commercial power supply operation at an inverter fault while the inverter running. Automatic switching is not available for the E.CPU.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700