Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21212
  • Release Date : 2018/08/22 16:26
  • Print

FR-HC2

Why did you start to recommend the fuse from the HC2? Can I use the breaker?
Category : 

Answer

It is fundamentally the same as the conventional model. Considering the recent safety awareness growth, we decided to start supporting it from the FR-HC2. Because the response speed of the breaker is slower than that of the fuse, the breaker cannot be used.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries