FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Changing the control method
FAQ
Changing the control method
I want to change the control method to Mitsubishi standard gear motor GM-D for the operation. Which parameters should I set when changing the control method?
- Category :
Answer
Set Pr.71 (Applied motor), Pr.80 (Motor capacity), Pr.81 (Number of motor poles), and Pr.800 (Control method selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700