FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Replacement
FAQ
Replacement
When the FR-A500 is replaced with FR-A700, which parameter number of the FR-A700 corresponds to Pr.903 (Frequency setting voltage gain) of FR-A500?
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
It is Pr.125 (Terminal 2 frequency setting gain frequency). Adjust the slope with C4 (903) (Terminal 2 frequency setting gain) as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700