FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Proportional band of multiple inverters
FAQ
Proportional band of multiple inverters
I want to perform proportional band of three inverters by changing the speed of one inverter. How should I input the inverter analog output to the second inverter?
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
By importing the operation frequency from the AM terminal (analog output) of the first inverter to the FR-FH (ratio setter), the operation command which is proportional to other three inverters can be sent.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700